38 Topic(s)
The AS-P server offers enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. The AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The AS-P controls and supervises equipment, typically HVAC equipment. AS-P servers use Central IO module with connected field devices, such as sensors and actuators, to do that.
These Central IO modules are digital output, Form A relay, 12-channel I/O modules. The Form A relays are designed for direct load applications for up to 2 A loads.
Part number: SXWTBIOW110002
For Central IO modules with outputs, the following components on the front provide control of the output channels:
By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.
This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.
There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.
The Central IO modules have the following status indicator LEDs on the front of the module:
The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.
You can wire a terminal base prior to installing an electronics module.