earth_america
user_standard Log on
action_search_stroke
earth_america

Mobile Apps

Commission
HMI Kiosk
SmartXKiosk
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

31 Topic(s)

Concept

There are a number of differences in functionality between Technician Tool and WebStation.

Concept

Custom View lists the objects and functions that are available in the Custom View folder of Building Operation in a logical manner, such as hierarchical, geographical, or functional. So, you do not see the entire tree structure of WorkStation, just the parts that you want to see or all the parts in the order that you want. For example, in WorkStation, you create a Custom View that contains variables of a Campus that you want to monitor from Technician Tool.

Concept

System displays the entire tree structure of Building Operation as it appears in WorkStation.

Specifications

User Interface

You use Settings to view the version of the product or edit the poll rate, number of decimals, trim long names, and set the time to automatically log off the SmartStruxure server when you are not accessing it. You can also select Alarms, System, or Custom View as the default tab. You can hide or see the system properties in System tree and Custom View tree.

How to

You acknowledge an alarm to let other users know that you have seen the alarm. When you log on to Technician Tool, the Alarms list is displayed. You can select and acknowledge multiple alarms.

Concept

Use Search to filter out the objects and variables in Custom View and System so that you do not have to browse through the long list of variables to locate the ones that concern you. Searches are folder based. You can search for the objects and variables within a particular folder.

How to

You save a search so that you can use it again.

Concept

Technician Tool is used to access the functions in Building Operation. You use Technician Tool to view and monitor all work on a daily basis in Building Operation. You can change the value for an event to control the output state of a device. You can also force a value when you want to override a value, such as a value from a device.

How to

For a faster log on, use the Remember me feature to automatically fill in your logon information.