earth_america
user_standard Log on
action_search_stroke
earth_america

PS-24V

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

30 Topic(s)

How to

You can wire a terminal base prior to installing an electronics module.

Concept

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).

User Interface

The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.

How to

You perform the following steps to power up a device.

Concept

Use the power budget to calculate the maximum number of devices that the power supply can supply. If more devices are used, additional power supplies must be added to the I/O bus.

Concept

The I/O bus is a common bus that delivers power, address information, and communication to all devices connected to the bus. The I/O bus is provided to the devices through the backplane in the terminal bases. The term I/O bus also denotes the chain of devices that are connected together.

Concept

The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.

Concept

The I/O bus consists of the following parts:

How to

You install an electronics module directly onto the relevant terminal base, where it will connect to the power supply and address bus.

How to

You install a terminal base on a horizontal DIN rail to ensure that the device is securely fastened and to allow sufficient cooling air flow through the electronics module. You install a terminal base on a DIN rail prior to connecting it to its neighboring terminal bases.