294 Topic(s)
Part number: SXWRCF16C10001
This section provides information on the external connectors that are required for the power supply input, outputs, and digital inputs of the RP controller expansion modules.
The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.
The KNX Modbus gateway RP-C-EXT-KNX connects to the RP-C controllers and provides an interface between the controller and KNX devices such as push-buttons, sensors, and control units for lights, blinds, and room temperature.
The RP-C-16A-M-24V model has 16 I/O points and the controller is equipped with 30 fixed screw terminals and a 3-position removable screw terminal block.
The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.
The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12B-M-24V model has 12 I/O points and the controller is equipped with 24 fixed screw terminals and a 3-position removable screw terminal block.
The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.
The RP-C-12A-M-24V model has 12 I/O points and the controller is equipped with 23 fixed screw terminals and a 3-position removable screw terminal block.