earth_america
user_standard Log on
action_search_stroke
earth_america

SpaceLogic Sensors

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

52 Topic(s)

Concept

The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Hardware Installation

How to

You connect SpaceLogic Sensor devices to an RP controller to provide the devices with power and communication from the controller.

How to

You connect SpaceLogic Sensor devices to an MP controller to provide the sensor devices with power and communication from the controller.

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

How to

In the SpaceLogic Sensor Touchscreen Display model, you change the occupancy mode to tell the control system that the room is occupied or unoccupied. You do so by enabling the Display object Occupancy override property. Depending on the control system programming, it may respond in various ways including changing the active setpoint from unoccupied to occupied, turning on the lights, and/or starting a timer that expires when the system becomes unoccupied again.

How to

You connect to a controller to begin all commissioning tasks. Through Bluetooth, you can connect to a single controller at a time. Bluetooth connectivity is supported for the MP and RP controllers of the BACnet/IP controller family. Bluetooth connectivity is not supported for IP-IO devices. On the MP controller you connect using the SpaceLogic BLE adapter through the controller’s sensor bus and Spacelogic Sensor. With RP controllers, you connect using the onboard BLE or the BLE adapter for the EasyLogic controller models.

How to

You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning. You configure the password for Bluetooth access in the RP controller.

How to

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to SpaceLogic and EasyLogic controller models. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.

Concept

When the room occupant presses the buttons on the SpaceLogic Sensor 3-Button Cover model to increase or decrease the temperature setpoint, the backlight changes from deep blue at the low end of the range, to deep red at the top end of the range. Each button push causes a 10% increase or decrease in the range. The backlight flashes rapidly three time to indicate the top or bottom of range has been reached.