341 Topic(s)
There are a number of different clients, servers, and features that requires licenses to operate.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
You add an exception event to configure an exception that is to apply instead of a scheduled weekly event for a single date, date range, or a time pair.
You add weekly events to a Xenta schedule to determine when the event is to regularly occur. Weekly events always occur regularly unless overridden by an exception event.
Use the Xenta Schedule Editor to view or edit Xenta schedules.
Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.
Use the Xenta Central Schedule Editor to add, view, or edit Xenta central schedules.
You edit an exception event to change the time range, start and stop date, start and stop time, or weekdays of an exception event.
Use the Building Operation WebStation window to log on to WebStation.
You edit a weekly event to change the time range, start and stop time, or weekdays of the weekly event.