361 Topic(s)
Use the Building Operation WebStation window to log on to WebStation.
You sort on alarms and events to get a better overview in the Alarms View or Events View.
You select fields in the Alarm view or Event view to display information regarding alarms and events.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.
Use the Select object dialog box to select the objects you want to add to the widget.
You add a trend log series to a trend chart to compare trend data from different logs or variables.
There are a number of different clients, servers, and features that requires licenses to operate.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.