405 Topic(s)
You add a single date exception event to make an exception for a specific day in the schedule, such as 10 December, 2013.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
There are a number of different clients, servers, and features that requires licenses to operate.
You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.
You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.
Use the User menu to access useful shortcuts from various menus in Workstation.
Content types are predefined layouts that you save to reuse for specific types of folders or container objects.
You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone automation server.