409 Topic(s)
You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.
You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
WorkStation is your main interface to your EcoStruxure BMS. You use WorkStation to perform all work on a daily basis in the EcoStruxure BMS.
You use Quick filter to filter out the objects by their names from the list. You can either type the name in the Quick filter box or drag an item from a column in the Alarms pane, the Events pane, an Alarm view, or an Event view and drop it in the Quick filter box.
Schedules are used to schedule the operation of parts of the BMS, such as a device or a setpoint. For example, a you can set up a schedule to make a device to operate between 08:00 and 17:00 every workday.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
The JavaScript utility object can be used by experienced software developers to increase reuse of JavaScript files.
Use the Add/Remove Columns dialog box to add or remove columns from the Alarms pane or an Alarm View.
The HTML utility object enables experienced software developers to embed custom web pages/applications inside the system.