The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. You plug the SpaceLogic Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller. The adapter communicates with the BACnet/IP controller over the sensor bus using an RS-485 cable. Więcej informacji zawiera Connecting SpaceLogic Sensor Devices to an MP Controller .
Więcej informacji zawiera Commission Mobile Application Overview .
You can use Bluetooth Low Energy (BLE) to connect both RP and MP controllers. BLE provides you with the ability to commission BACnet/IP controllers before there is an IP network infrastructure configured and also improves on-site commissioning times and productivity. With the RP controller, you connect using its onboard BLE or the BLE adapter and the SpaceLogic Sensor. In the MP controller, you connect using the Commission mobile application BLE adapter through the controller's sensor bus.
Więcej informacji zawiera RP Controller Onboard BLE .
The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.
Więcej informacji zawiera Connecting to a Controller with the SpaceLogic Bluetooth Adapter .
You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The SpaceLogic Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning.
Więcej informacji zawiera Changing the PIN of the SpaceLogic Bluetooth Adapter .
You update the SpaceLogic Bluetooth Adapter firmware to improve adapter performance.
Więcej informacji zawiera Updating the SpaceLogic Bluetooth Adapter Firmware .
You perform a factory reset on the SpaceLogic Bluetooth Adapter to erase the current PIN.
Więcej informacji zawiera Performing a Factory Reset on the Bluetooth Adapter .
The SpaceLogic Bluetooth Adapter LED light displays different sequences to indicate the various functionality.
Więcej informacji zawiera Bluetooth LED Functionality .