earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: eCommission SmartX Controllers, MP-C, MP-V, RP-C, SmartX Sensor
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 3.3
2021-12-17

SpaceLogic Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. You plug the SpaceLogic Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller. The adapter communicates with the BACnet/IP controller over the sensor bus using an RS-485 cable. Mer information finns i Connecting SpaceLogic Sensor Devices to an MP Controller .

Obs!

SPACELOGIC SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SpaceLogic Sensor.

Failure to follow these instructions can result in equipment damage.

Mer information finns i eCommission SmartX Controllers Mobile Application Overview .

 
action_zoom_plus_stroke SpaceLogic Bluetooth Adapter connectivity
Figur: SpaceLogic Bluetooth Adapter connectivity

RP Controller Onboard BLE

You can use Bluetooth Low Energy (BLE) to connect both RP and MP controllers. BLE provides you with the ability to commission BACnet/IP controllers before there is an IP network infrastructure configured and also improves on-site commissioning times and productivity. With the RP controller, you connect using its onboard BLE or the BLE adapter and the SpaceLogic Sensor. In the MP controller, you connect using the eCommission SmartX Controller mobile application BLE adapter through the controller's sensor bus.

Mer information finns i RP Controller Onboard BLE .

Connecting to a Controller with the SpaceLogic Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.

Mer information finns i Connecting to a Controller with the SpaceLogic Bluetooth Adapter .

Changing the PIN of the SpaceLogic Bluetooth Adapter

You change the PIN of the SpaceLogic Bluetooth Adapter for best security practices. The SpaceLogic Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning.

Mer information finns i Changing the PIN of the SpaceLogic Bluetooth Adapter .

Updating the SpaceLogic Bluetooth Adapter Firmware

You update the SpaceLogic Bluetooth Adapter firmware to improve adapter performance.

Mer information finns i Updating the SpaceLogic Bluetooth Adapter Firmware .

Performing a Factory Reset of the SpaceLogic Bluetooth Adapter

You perform a factory reset on the SpaceLogic Bluetooth Adapter to erase the current PIN.

Mer information finns i Performing a Factory Reset on the Bluetooth Adapter .

SpaceLogic Bluetooth Adapter LED Functionality

The SpaceLogic Bluetooth Adapter LED light displays different sequences to indicate the various functionality.

Mer information finns i Bluetooth LED Functionality .

  • eCommission SmartX Controllers Mobile Application Overview
  • RP Controller Onboard BLE
  • Connecting to a Controller through Bluetooth
  • Changing the PIN of the SpaceLogic Bluetooth Adapter
  • Updating the SpaceLogic Bluetooth Adapter Firmware
  • Performing a Factory Reset on the Bluetooth Adapter
  • Bluetooth LED Functionality