It is important to perform the grounding correctly for the following reasons:
To design a system that is not harmed by detected minor connection errors.
To design a system that works well and is resistant to EMI.
To minimize the effects of ground currents that can cause unstable measurements.
The following sections provide recommendations for designing a good working system.
This section provides grounding and power recommendations for system configurations with Central IO modules and PS-24V units.
Mer information finns i Grounding and Power for Systems with Central IO Modules and PS-24V Units .
This section provides grounding and power recommendations for system configurations with AS-B servers.
Mer information finns i Grounding and Power for Systems with AS-B Servers .
This section provides grounding and power recommendations for system configurations with MP controllers.
Mer information finns i Grounding and Power for Systems with MP Controllers .
This section provides grounding and power recommendations for system configurations with IP-IO modules.
Mer information finns i Grounding and Power for Systems with IP-IO Modules .
This section provides grounding and power recommendations for system configurations with the RP-C controller models RP-C-12A, -12B, or -12C, which are models that support 24 VAC/DC input power.
Mer information finns i Grounding and Power for Systems with RP-C-12A, -12B, or -12C Controllers .
This section provides grounding and power recommendations for system configurations with the RP-C controller model RP-C-16A, which is a model that supports 230 VAC input power.
Mer information finns i Grounding and Power for Systems with RP-C-16A Controller .
This section provides grounding and power recommendations for system configurations with an RP-C and RP controller expansion modules.
Mer information finns i Grounding and Power for Systems with RP-C-16A and Expansion Modules .
This section provides grounding and power recommendations for system configurations with Operator Display, which supports 24 VDC input power.
Mer information finns i Grounding and Power for Systems with Operator Display .