You edit system installation information to update or correct the information. The Schneider Electric partner or branch user cannot edit information if the system is associated to the end-user.
When information is updated, an email is sent to the registered user, partner, or branch user and the site administrator.
Log on to the SmartStruxure Solution Registration Portal.
Click Systems .
Under Registered Systems ,select the system.
Select the Installation tab and click Edit .
Edit the information as required.
Property |
Description |
System ID |
Displays system Id of the registered system |
Registration code |
Displays registration code generated by SmartStruxure Registration Portal after successful system registration process. |
Site type |
Select the system type. If there is only one SmartStruxure server installed at the site, select Single site option. If there are more than one Enterprise Servers installed at the site, select Multi site option. |
Site/building name |
Type the site/building name. |
Site company name |
Type the company name. |
System transition (if applicable) |
Select the systems that existed before installing Building Operation System on the site. |
System application |
Select the applications to which the system is commissioned for. |
Segment/application |
Select the business segments you belong to. |
Installation address |
Type the site/building address where the system is installed. |
Country |
Type the country to which site/building belongs. |
State/province |
Type the state or province to which site/building belongs. |
City |
Type the city. |
Zip/postal code |
Type the zip/postal code of the region where site is located. |
Click Submit .