Productos AS-B, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2
02/10/2024

Duplicating a SmartX Server Using Restore 

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone SmartX server.

Aviso

Restoring with new ID does not work if the database contains a BACnet interface.

The locally stored backup set and the SmartX server need to have the same password.

Mostrar más
action_close

You can use the Restore function to re-use the configuration data from a backup set in a new standalone SmartX server. Rather than manually configuring your preferred SmartX server configuration, you can save time and configure the standalone SmartX server from a backup set.

The backup set used can originate from a SmartX server that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

Para obtener más información, consulte Backup Sets .

Protocol Compatibility

The restore function to re-use configuration data from a backup set is supported for all protocols supported by EcoStruxure Building Operation software, except for BACnet and b3 BACnet.

LonWorks Devices Neuron IDs deleted on duplicated SmartX server

The LonWorks devices connected to the SmartX server are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from a SmartX server, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new SmartX server.

Para obtener más información, consulte LonWorks Device Workflows .

Password deleted on duplicated EcoStruxure BMS device

When you duplicate a SmartX device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server Site

To create a new SmartX server in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new SmartX server to the Enterprise Server and select the backup set in the Create Object Wizard.

Para obtener más información, consulte Creating a SmartX Server from a Backup Set .

Standalone SmartX Server Site

You use a locally stored backup set to duplicate another SmartX server configuration in a standalone SmartX server. You then import the backup set to a client and restore to the new standalone SmartX server.

Para obtener más información, consulte Duplicating a SmartX Server Using Restore  .

Duplicate SmartX Server from a Backup Set Workflow

Use the following workflow to duplicate a SmartX server from a backup set.

 
action_zoom_plus_stroke Duplicate SmartX server using restore flowchart
Figura: Duplicate SmartX server using restore flowchart
Backup a SmartX server

Backup a SmartX server that has the configuration you want to use in the new standalone SmartX server.

Para obtener más información, consulte Backing Up EcoStruxure BMS Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

Para obtener más información, consulte Saving a SmartX Server Backup Set to Another Location .

Log on to standalone SmartX server

Log on to a new standalone SmartX server.

Para obtener más información, consulte Inicio de sesión en WorkStation como usuario de EcoStruxure Building Operation .

Import backup set

Import the backup set.

Para obtener más información, consulte Importing a Backup Set to SmartX Server .

Restore SmartX server using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone SmartX server. The communication settings from the backup set are not duplicated.

Para obtener más información, consulte Duplicating a SmartX Server Using Restore  .

Aviso

When you restore a standalone SmartX server, you are logged off and need to log on manually after the restore is complete.

To duplicate a SmartX server using restore
  1. In WorkStation, in the System Tree pane, select the server where you want to duplicate configuration data from a backup set.

  2. On the Actions menu, click Restore .

  3. In the Restore Options dialog box, in the Available restore points list, select the backup set.

  4. Select Restore configuration with new IDs checkbox to re-use the configuration data from the backup set in a new standalone SmartX server.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

  • Duplicate SmartX Server from a Backup Set
  • Restore
  • Restore Options Dialog Box
  • Importing a Backup Set to SmartX Server
  • Backup Set Text is Red