earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, AS-P, WorkStation, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/3

Duplicating a Field Server Using Restore 

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone field server.

重要:

The locally stored backup set and the field server need to have the same password.

Restoring with new ID does not work if the database contains a BACnet interface.

显示更多
action_close

You can use the Restore function to re-use the configuration data from a backup set in a new standalone field server. Rather than manually configuring your preferred field server configuration, you can save time and configure the standalone field server from a backup set.

The backup set used can originate from a field server that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

有关更多信息,请参阅 Backup Sets .

Protocol compatibility

The restore function to re-use configuration data from a backup set is supported for all protocols supported by EcoStruxure Building Operation software, except for BACnet and b3 BACnet.

LonWorks devices Neuron IDs deleted on duplicated field server

The LonWorks devices connected to the field server are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from a field server, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new field server.

有关更多信息,请参阅 LonWorks Device Workflows .

Password deleted on duplicated EcoStruxure BMS device

When you duplicate a SpaceLogic device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server site

To create a new field server in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new field server to the Enterprise Server and select the backup set in the Create Object Wizard.

有关更多信息,请参阅 Creating a Field Server from a Backup Set .

Standalone field server site

You use a locally stored backup set to duplicate another field server configuration in a standalone field server. You then import the backup set to a client and restore to the new standalone field server.

有关更多信息,请参阅 Duplicating a Field Server Using Restore  .

Duplicate Field Server from a Backup Set Workflow

Use the following workflow to duplicate a field server from a backup set.

 
action_zoom_plus_stroke Duplicate Field Server using restore flowchart
图: Duplicate Field Server using restore flowchart
Backup a field server

Backup a field server that has the configuration you want to use in the new standalone field server.

有关更多信息,请参阅 Backing Up EcoStruxure BMS Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

有关更多信息,请参阅 Saving a Field Server Backup Set to Another Location .

Log on to standalone field server

Log on to a new standalone field server.

有关更多信息,请参阅 Logging on to WorkStation as an EcoStruxure Building Operation User .

Import backup set

Import the backup set.

有关更多信息,请参阅 Importing a Backup Set to Field Server .

Restore field server using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone field server. The communication settings from the backup set are not duplicated.

有关更多信息,请参阅 Duplicating a Field Server Using Restore  .

重要:

When you restore a standalone field server, you are logged off and need to log on manually after the restore is complete.

To duplicate a field server using restore
  1. In WorkStation, in the System Tree pane, select the server where you want to duplicate configuration data from a backup set.

  2. On the Actions menu, click Restore .

  3. In the Restore Options dialog box, in the Available restore points list, select the backup set.

  4. Select Restore configuration with new IDs checkbox to re-use the configuration data from the backup set in a new standalone field server.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

  • Duplicate Field Server from a Backup Set
  • Restore
  • Restore Options Dialog Box
  • Importing a Backup Set to Field Server
  • Backup Set Text is Red