earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2023
2022/12/16

Configuring Connect Agent Settings

You configure the Connect Agent Settings to enable the agent to transfer the crash information of the EcoStruxure BMS servers to the Connect storage server.

显示更多
action_close

Connect Agent is the service that runs along with the Enterprise Central and Enterprise Servers attached to it to collect and transfer crash information of EcoStruxure BMS servers (Enterprise Central, Enterprise Servers and automation servers attached to Enterprise Servers).

To transfer the crash information, the Connect Agent service Log on needs to meet the following conditions:

  • sufficient user rights to access system folders and internet

  • Internet proxy settings, if required

  • Port number 22 available to access the following URL: servercd.smartstruxure.schneider-electric.com

Connect Agent can collect and transfer crash information only when the site administrator or the end-user provides consent to allow Schneider Electric to receive system diagnostic and performance data of the system.

To enable the Connect Agent function, set Enable crash information transfer to True. 有关更多信息,请参阅 Configuring Connect Agent Settings .

To configure Connect Agent Settings
  1. In WorkStation, in the System Tree pane, expand the System folder.

  2. Expand the Connect Settings folder and select Connect Agent Settings .

  3. On the File menu, click Properties .

  4. In the Enable crash information transfer box, select True .

  5. Click the Advanced tab.

  6. In Maximum bandwidth box, select the maximum bandwidth at which the crash information can be transfered. If '0' is selected, the crash information is transfered at maximum bandwidth.

  • Connect Agent Overview
  • Connect Agent Settings - Basic Tab
  • Connect Agent Settings - Advanced Tab