earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 3.3, 2022
12/14/2022

Adding an Automation Server to the Whitelist

You add a device to the whitelist so that it can communicate with the automation server.

Show More
action_close

You can configure the devices that are allowed to communicate with the automation server to prevent connection attempts from unauthorized devices. The IP addresses of the devices that are allowed to communicate with the automation server are added to the whitelist.

The devices IP addresses are specified in the whitelist by their IP addresses or by specifying an address mask that includes the devices address. This makes it possible to add a mask of IP addresses to the whitelist using CIDR notation. The whitelist can be edited at any time.

The default whitelist, 0.0.0.0/0, allows all devices to communicate with the automation server. When you add devices to the whitelist, only the devices on the whitelist can communicate.

The maximum allowed size of a whitelist is 2048 bytes, approximately 100 devices.

Notice

Loss of data

When you start to add devices to the whitelist using a network connection, make sure that you add the computer you are using to the whitelist. If you do not add the computer you are using to the whitelist, you lock yourself out from the automation server.

If you lock yourself out, you can connect to the automation server using the USB and then reset the whitelist. For more information, see Connecting to an Automation Server Using the USB Device Port .

Failure to follow these instructions can result in loss of data.

Notice

Loss of data

When you start to add devices to the whitelist using a network connection, make sure that you add the computer you are using to the whitelist. If you do not add the computer you are using to the whitelist, you lock yourself out from the automation server.

If you lock yourself out, you can connect to the automation server using the USB and then reset the whitelist. For more information, see Connecting to an Automation Server Using the USB Device Port .

Failure to follow these instructions can result in loss of data.

To add a device to the whitelist
  1. In Device Administrator, click Servers and then click the server.

  2. Click Firewall .

  3. In the Whitelist box, type the IP numbers. A whitespace is required between every IP address in the list.

    Tip:

    To add a complete subnet of IP addresses, add the subnet according to the CIDR network prefix notation syntax.

  4. Click OK .

  • Firewall
  • Firewall Tab
  • Removing a Device from the Whitelist