earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos Enterprise Server, Project Configuration Tool
Funcionalidades: Gestión de usuarios
Versión del producto: 1.9
14/12/2016

Removing Software Permissions from a User Account Group

You remove a user account goup's path permission to remove the permission to a folder or an object the user account group no longer is to have permissions to.

Mostrar más
action_close

A user account group can comprise both user accounts and other user account groups with similar interests. By using a well planned strategy for your user account groups, you apply software ​permissions and polices to multiple user accounts.

For optimal efficiency, assign software permissions to user account groups rather than individual user accounts, wherever possible. Using this approach, you can associate user accounts to at least one user account group for controlled permission to Building Operation applications. For instance, you can group software permissions with user accounts based on common tasks and responsibilities​

You create user accounts groups and then apply one or more software permissions. For example, create a user account for Paul and associate him with the two user account groups: Administrators and Janitors. Paul inherits the software permissions of both user account groups. You can also set up general policies for the user accounts that are members to the user account group. For example, you can enable or disable the ability of group members to change their passwords or to close the User Interface. Para obtener más información, consulte Software Permissions .

 
action_zoom_plus_stroke Users inherit the user account group permissions of which they are members
Figura: Users inherit the user account group permissions of which they are members

Paul and Susan are members of the Janitor user account group, which includes an Operator workspace and a set of software permissions. The Janitor group is also a member of the Operator group. Therefore, the Janitor group inherits the settings and workspaces of the Operator group. In other words, Paul and Susan share the software permissions of both the Janitor and the Operator groups, and have access to the Operator and Janitor workspaces.

 
action_zoom_plus_stroke Software permissions and workspaces are assigned to user account groups
Figura: Software permissions and workspaces are assigned to user account groups

To remove software permissions from a user account group
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Account management .

  4. In the Domain list, select the domain the user account group belongs to.

     
    action_zoom_plus_stroke
  5. In the User Account Groups list, select the user account group whose path permissions you want to remove.

  6. Click Software Permissions .

  7. In the Path list, select the path whose permissions you want to remove from the user account group.

     
    action_zoom_plus_stroke
  8. Click the Remove button

     
    action_zoom_plus_stroke
    .

  • Software Permissions and User Account Groups
  • Software Permissions
  • Assigning Software Permissions to a User Account Group
  • Editing the Software Permissions of a User Account Group
  • Restricting the Permission to Change the Alarm State Sort Order
  • User Account Group – Software Permissions Tab
  • Removing Path Permissions from a User Account
  • Account Management Control Panel
  • Software Permission Rules