earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-P Smoke Control, Automation Server Smoke Control
Funzionalità: Smoke Control
Versione del prodotto: 1.8
26/09/2016

MNA-FLO-1 Enclosure

arrow1_rotationFront View arrow1_rotationInside View arrow1_rotationPhysical Dimensions arrow1_rotationMounting Dimensions

The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.

Front View

The following illustration shows the front view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Panel
Figura: MNA-FLO-1 Enclosure - Front Panel

As shown, the front view includes a product and smoke control label and an enclosure cover.

Inside View

The following illustration shows the inside view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Inside View
Figura: MNA-FLO-1 Enclosure - Inside View

As shown, the inside of the enclosure includes a b3865-V-S controller, an enclosure base, a damper shaft, a product label, and a mounting tab.

Physical Dimensions

The following illustration shows the physical dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Dimensions
Figura: MNA-FLO-1 Enclosure - Front Dimensions

The MNA-FLO-1 provides knockouts in the positions shown for .50 inches (12.70 mm) or .75 inches (19.05 mm) conduit connections.

Mounting Dimensions

The following illustration shows the mounting dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Mounting Dimensions
Figura: MNA-FLO-1 Enclosure - Mounting Dimensions
  • Smoke Control Recommended Enclosures
  • UNM-SCH13186RC Enclosure
  • UNM-SCH181810RC Enclosure
  • UNM-SCH242410RC Enclosure
  • UNM-SCH243610RC Enclosure
  • UNM-SCH303610RC Enclosure
  • UNM-SCH304810RC Enclosure
  • UL 864 Smoke Control Enclosure Mounting Hardware
  • Mounting a UL 864 Smoke Control Enclosure