earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-P Smoke Control, Automation Server Smoke Control
Funzionalità: Hardware, Smoke Control
Versione del prodotto: 1.8
26/09/2016

UNM-SCH181810RC Enclosure

arrow1_rotationFront View arrow1_rotationInside View arrow1_rotationPhysical Dimensions arrow1_rotationMounting Dimensions

The UNM-SCH181810RC enclosure is a 10-inch deep box (254.00 mm) box with a continuous hinge, keyed door lock, compression latch, and a perforated back pane. It is designed for use with StruxureWare Building Operation components, such as Automation Servers, Power Supplies, and Input/Output modules.

Front View

The following illustration shows the front view of the enclosure.

 
action_zoom_plus_stroke UNM-SCH181810RC Enclosure - Front View
Figura: UNM-SCH181810RC Enclosure - Front View

The UNM-SCH181810RC enclosure does not feature DIN rails. However, you can fasten them with screws through the pre-drilled backplane. A keylock is provided for added security.

Inside View

The following illustration shows the inside view of the enclosure.

 
action_zoom_plus_stroke UNM-SCH181810RC Enclosure - Inside View
Figura: UNM-SCH181810RC Enclosure - Inside View

As shown, the inside of the enclosure includes the perforated back panel.

Physical Dimensions

The following illustration shows the physical dimensions of the enclosure.

 
action_zoom_plus_stroke UNM-SCH181810RC Enclosure - Physical Dimensions
Figura: UNM-SCH181810RC Enclosure - Physical Dimensions

Mounting Dimensions

The following illustration shows the mounting dimensions of the enclosure.

 
action_zoom_plus_stroke UNM-SCH1818110RC Enclosure - Mounting Dimensions
Figura: UNM-SCH1818110RC Enclosure - Mounting Dimensions
  • Smoke Control Recommended Enclosures
  • MNA-FLO-1 Enclosure
  • UNM-SCH13186RC Enclosure
  • UNM-SCH242410RC Enclosure
  • UNM-SCH243610RC Enclosure
  • UNM-SCH303610RC Enclosure
  • UNM-SCH304810RC Enclosure
  • UL 864 Smoke Control Enclosure Mounting Hardware
  • Mounting a UL 864 Smoke Control Enclosure