The UNM-SCH303610RC enclosure is a 10-inch deep box (254.00 mm) box with a continuous hinge, keyed door lock, compression latch, and a perforated back pane. It is designed for use with StruxureWare Building Operation components, such as Automation Servers, Power Supplies, and Input/Output modules.
The following illustration shows the front view of the enclosure.
The UNM-SCH303610RC enclosure does not feature DIN rails. However, you can fasten them with screws through the pre-drilled backplate. A keylock is provided for added security.
The following illustration shows the inside view of the enclosure.
As shown, the inside of the enclosure includes the perforated back panel.
The following illustration shows the physical dimensions of the enclosure.
The following graphic shows the mounting dimensions of the enclosure.