earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funzionalità: Allarmi, Funzionalità di base
Versione del prodotto: 1.8
14/10/2016

Adding to Favorites

You add a favorite to save a layout and filter change that you have made to the Alarms pane, Events pane, Alarm View, or Event View.

Avviso

You have to be logged on to the domain controller of the domain where you want to make the filter or layout changes to be able to access the Favorites feature.

Mostra di più
action_close

When you make layout or filter changes to the Alarms pane, Events pane, an Alarm View, or Event View, you can save the changes as a favorite. The purpose of the favorite is to quickly and temporarily change the Standard layout and narrow what is displayed in the pane or View by applying the favorite filter conditions.

Avviso

You have to be logged on to the domain controller of the domain where you want to make the filter or layout changes to be able to access the Favorites feature.

A favorite is saved for the logged on user account and is available from any computer in the Building Operation system.

When you apply a favorite, the layout and content of the pane or View changes according to the favorite layout and filter conditions. A favorite cannot display information the logged on user account does not have permissions to see. When you apply a favorite, you do not alter the pane or View for anyone else who is currently logged on using the same user account.

You can rename an existing favorite or edit the layout and filter conditions of an applied favorite and save it under the existing or a new name. You can also delete a favorite. When you delete a favorite, you do not alter the pane or View for anyone else who is currently logged on using the same user account.

You can return to the Standard layout and filter at any time. When you log off and log back on, the pane or View returns to the Standard layout and filter.

To add to favorites
  1. On the Alarms pane, Events pane, Alarm View , or Event View . toolbar, click the Favorites button

     
    action_zoom_plus_stroke
    .

  2. Click Add to favorites .

  3. In the Name box, type a name for the favorite.

     
    action_zoom_plus_stroke
  4. Click OK .

The current layout and user filter are saved as a favorite and are displayed on the Favorites menu.

  • Favorites
  • Applying a Favorite
  • Renaming a Favorite
  • Deleting a Favorite
  • Finestra di dialogo Salva preferito
  • Favorites Menu