earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: AS-B, AS-P
Funktionaliteter: Programmering, Säkerhet
Produktversion: 2023, 2024, 7.0
2024-11-14

Disabling Port 22 on an Automation Server

You disable port 22 on your automation server to avoid cyber-attack on this port.

Visa mer
action_close

You can disable port 22 and the USB ports on the automation server.

Port 22

Port 22 is used for communication with Device Administrator. This port is often the target for cyber-attacks. You can disable this port or change the port so that the automation server communicates on another port using SSH. You can also disable all SSH communication.

Mer information finns i Disabling Port 22 on an Automation Server .

Mer information finns i Adding an Additional SSH Port for an automation Server .

USB port

To prevent anyone from tampering with your automation servers on site you can disable the USB ports.

The USB ports can be disabled on both the AS-B and AS-P servers but not on the automation server AS. The setting is visible on the automation server AS but grayed out and cannot be changed.

Mer information finns i Disabling the USB Port on an Automation Server  .

To disable port 22 on an automation server
  1. In WorkStation, in the System Tree pane, select the automation server.

  2. Click the Properties tab.

  3. Click the Network tab.

  4. Expand Port Settings .

  5. In the Default SSH port (22) list, click Disable .

  6. Click Save .

  • Disable Automation Server Ports