Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Change of State Alarm Properties – Alarm Settings Tab

Use the ​ Alarm Settings tab to change the alarm properties of a change of state alarm.

 
action_zoom_plus_stroke Alarm Settings tab
Rysunek: Alarm Settings tab

Tabela: Alarm Settings Tab

Property

Description

Acknowledgement type

Select the type of acknowledgement for the alarm.

Więcej informacji zawiera Acknowledgements .

Alarm message

Type the message to display when the alarm is in Alarm state.

Więcej informacji zawiera Alarm Messages .

Reset message

Type the message to display when the alarm is reset.

Alarm priority

Enter the priority level of the alarm.

Więcej informacji zawiera Alarm Priority .

Reset priority

Enter the priority level of the alarm when it is reset.

Więcej informacji zawiera Alarm Priority .

Category

Enter the category the alarm belongs to.

Więcej informacji zawiera Alarm Categories .

Category 2

Enter the second category the alarm belongs to.

Więcej informacji zawiera Alarm Categories .

Cause note group

Enter the cause note group used by the alarm.

Więcej informacji zawiera Cause Notes .

Action note group

Enter the action note group used by the alarm.

Więcej informacji zawiera Action Notes .

Checklist

Enter the checklist that belongs to the alarm.

Więcej informacji zawiera Checklists .

Checklist required

Select to require that a checklist is filled in before acknowledging the alarm.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Disable alarm

Select to disable the alarm, for example, before deployment.

Więcej informacji zawiera Disable and Enable Alarms .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Więcej informacji zawiera Hide and Show Alarms .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

Więcej informacji zawiera Alarm State-Change Logging .

F lashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggerd.

Custom audio

Enter the path to the custom audio file you want to play when the alarm is triggered.

 
action_zoom_plus_stroke
(Action Requirements)

Edit

Click to open the property pane where you edit the selected user action.

Więcej informacji zawiera User Action Properties .

 
action_zoom_plus_stroke
(Attachments)

Add

Click to open the Create Object: Attachment wizard where you add an attachment.

Więcej informacji zawiera Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke
(Attachments)

Edit

Click to open the property pane where you configure the attachment.

Więcej informacji zawiera Attachment Properties .

 
action_zoom_plus_stroke
(Attachments)

Remove

Click to remove an attachment that is connected to the alarm.

  • Change of State Alarms
  • Change of State Alarm Properties – Basic Tab
  • References Tab
  • Acknowledgements
  • Alarm Messages
  • Priorities
  • Alarm Categories
  • Cause Notes
  • Action Notes
  • Checklists
  • Disable and Enable Alarms
  • Hide and Show Alarms
  • Alarm State-Change Logging
  • Custom Audible Alarm Alerts
  • User Action Properties
  • Create Object Dialog – Naming the Object Page
  • Attachment Properties
  • Alarms Substitution Codes