Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

User Action Properties

Use the User Action properties dialog box to configure the mandatory or required user actions items.

 
action_zoom_plus_stroke User action properties
Rysunek: User action properties

Tabela: User Action Properties

Component

Description

User action

Displays the user action item you are configuring.

Comment

Select True to require the users to write a comment when they perform this kind of user action.

Action note

Select True to require the users to add an action note to this kind of user action.

Cause note

Select True to require the users to report the circumstances of this kind of user action.

  • User Actions
  • Create Alarm Wizard – User Action Page