Use the Alarm Settings tab to change the alarm properties of a multistate alarm.
Property |
Description |
Acknowledgement type |
Select the type of acknowledgement for the alarm. Więcej informacji zawiera Acknowledgements . |
Alarm message |
Type the message to display when the alarm is in Alarm state. Więcej informacji zawiera Alarm Messages . |
Reset message |
Type the message to display when the alarm is reset. |
Alarm priority |
Enter the priority level of the alarm. Więcej informacji zawiera Alarm Priority . |
Reset priority |
Enter the priority level of the alarm when it is reset. Więcej informacji zawiera Alarm Priority . |
Category |
Enter the category the alarm belongs to. Więcej informacji zawiera Alarm Categories . |
Category 2 |
Enter the second category the alarm belongs to. Więcej informacji zawiera Alarm Categories . |
Cause note group |
Enter the cause note group used by the alarm. Więcej informacji zawiera Cause Notes . |
Action note group |
Enter the action note group used by the alarm. Więcej informacji zawiera Action Notes . |
Checklist |
Enter the checklist that belongs to the alarm. Więcej informacji zawiera Checklists . |
Checklist required |
Select to require that a checklist is filled in before acknowledging the alarm. |
Prefix for alarm source name |
Type a prefix that is added to the beginning of the source name property of an alarm record. |
Disable alarm |
Select to disable the alarm, for example, before deployment. Więcej informacji zawiera Disable and Enable Alarms . |
Auto hide |
Select to automatically hide the alarm in the Alarms pane or Alarm View. Więcej informacji zawiera Hide and Show Alarms . |
Disable state-change logging |
Select to prevent an alarm state change from creating an event. Więcej informacji zawiera Alarm State-Change Logging . |
F lashing alert |
Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered. |
Audible alert |
Select to make the alert audible when the alarm is triggerd. |
Custom audio |
Enter the path to the custom audio file you want to play when the alarm is triggered. |
|
Edit Click to open the property pane where you edit the selected user action. Więcej informacji zawiera User Action Properties . |
|
Add Click to open the Create Object: Attachment wizard where you add an attachment. Więcej informacji zawiera Create Object Dialog – Naming the Object Page . |
|
Edit Click to open the property pane where you configure the attachment. Więcej informacji zawiera Attachment Properties . |
|
Remove Click to remove an attachment that is connected to the alarm. |