16/12/2022

Sum Alarm Properties – Alarm Settings Tab

Use the ​ Alarm Settings Tab tab to change the alarm properties of a sum alarm.

 
action_zoom_plus_stroke Alarm Settings tab
Figura: Alarm Settings tab

Tabella: Alarm Settings Tab

Property

Description

Acknowledgement type

Select the type of acknowledgement for the alarm.

Per maggior informazioni, consulta Acknowledgements .

Alarm message

Type the message to display when the alarm is in Alarm state.

Per maggior informazioni, consulta Alarm Messages .

Reset message

Type the message to display when the alarm is reset.

Alarm priority

Enter the priority level of the alarm.

Per maggior informazioni, consulta Alarm Priority .

Reset priority

Enter the priority level of the alarm when it is reset.

Per maggior informazioni, consulta Alarm Priority .

Category

Enter the category the alarm belongs to.

Per maggior informazioni, consulta Alarm Categories .

Category 2

Enter the second category the alarm belongs to.

Per maggior informazioni, consulta Alarm Categories .

Cause note group

Enter the cause note group used by the alarm.

Per maggior informazioni, consulta Cause Notes .

Action note group

Enter the action note group used by the alarm.

Per maggior informazioni, consulta Action Notes .

Checklist

Enter the checklist that belongs to the alarm.

Per maggior informazioni, consulta Checklists .

Checklist required

Select to require that a checklist is filled in before acknowledging the alarm.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Disable alarm

Select to disable the alarm, for example, before deployment.

Per maggior informazioni, consulta Disattivazione e attivazione allarmi .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Per maggior informazioni, consulta Mostra e nascondi allarmi .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

Per maggior informazioni, consulta Registrazione del cambio di stato di un allarme .

F lashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggerd.

Custom audio

Enter the path to the custom audio file you want to play when the alarm is triggered.

 
action_zoom_plus_stroke
(Action Requirements)

Edit

Click to open the property pane where you edit the selected user action.

Per maggior informazioni, consulta User Action Properties .

 
action_zoom_plus_stroke
(Attachments)

Add

Click to open the Create Object: Attachment wizard where you add an attachment.

Per maggior informazioni, consulta Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke
(Attachments)

Edit

Click to open the property pane where you configure the attachment.

Per maggior informazioni, consulta Attachment Properties .

 
action_zoom_plus_stroke
(Attachments)

Remove

Click to remove an attachment that is connected to the alarm.

  • Sum Alarms
  • Sum Alarm Properties – Basic Tab
  • References Tab
  • Acknowledgements
  • Alarm Messages
  • Alarm Priority
  • Alarm Categories
  • Cause Notes
  • Action Notes
  • Checklists
  • Disattivazione e attivazione allarmi
  • Mostra e nascondi allarmi
  • Registrazione del cambio di stato di un allarme
  • Custom Audible Alarm Alerts
  • User Action Properties
  • Create Object Dialog – Naming the Object Page
  • Attachment Properties
  • Alarms Substitution Codes