earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2019/1/3

Sum Alarm Properties – Alarm Settings Tab

Use the ​ Alarm Settings Tab tab to change the alarm properties of a sum alarm.

 
action_zoom_plus_stroke Alarm Settings tab
图: Alarm Settings tab

表格: Alarm Settings Tab

Property

Description

Acknowledgement type

Select the type of acknowledgement for the alarm.

有关更多信息,请参阅 Acknowledgements .

Alarm message

Type the message to display when the alarm is in Alarm state.

有关更多信息,请参阅 Alarm Messages .

Reset message

Type the message to display when the alarm is reset.

Alarm priority

Enter the priority level of the alarm.

有关更多信息,请参阅 Alarm Priority .

Reset priority

Enter the priority level of the alarm when it is reset.

有关更多信息,请参阅 Alarm Priority .

Category

Enter the category the alarm belongs to.

有关更多信息,请参阅 Alarm Categories .

Category 2

Enter the second category the alarm belongs to.

有关更多信息,请参阅 Alarm Categories .

Cause note group

Enter the cause note group used by the alarm.

有关更多信息,请参阅 Cause Notes .

Action note group

Enter the action note group used by the alarm.

有关更多信息,请参阅 Action Notes .

Checklist

Enter the checklist that belongs to the alarm.

有关更多信息,请参阅 Checklists .

Checklist required

Select to require that a checklist is filled in before acknowledging the alarm.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Disable alarm

Select to disable the alarm, for example, before deployment.

有关更多信息,请参阅 禁用和启用报警 .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

有关更多信息,请参阅 隐藏和显示报警 .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

有关更多信息,请参阅 报警状态更改记录 .

F lashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggerd.

Custom audio

Enter the path to the custom audio file you want to play when the alarm is triggered.

 
action_zoom_plus_stroke
(Action Requirements)

Edit

Click to open the property pane where you edit the selected user action.

有关更多信息,请参阅 User Action Properties .

 
action_zoom_plus_stroke
(Attachments)

Add

Click to open the Create Object: Attachment wizard where you add an attachment.

有关更多信息,请参阅 Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke
(Attachments)

Edit

Click to open the property pane where you configure the attachment.

有关更多信息,请参阅 Attachment Properties .

 
action_zoom_plus_stroke
(Attachments)

Remove

Click to remove an attachment that is connected to the alarm.

  • Sum Alarms
  • Sum Alarm Properties – Basic Tab
  • References Tab
  • Acknowledgements
  • Alarm Messages
  • Alarm Priority
  • Alarm Categories
  • Cause Notes
  • Action Notes
  • Checklists
  • 禁用和启用报警
  • 隐藏和显示报警
  • 报警状态更改记录
  • Custom Audible Alarm Alerts
  • User Action Properties
  • Create Object Wizard – Naming the Object Page
  • Attachment Properties
  • Alarm Substitution Codes