earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2021/5/4

Attachment Properties

Use the Attachment properties to edit attachments and configure whether or not the attachments are displayed when the alarm is triggered.

 
action_zoom_plus_stroke Attachment properties
图: Attachment properties

表格: Attachment Properties

Component

Description

Display on alarm

Select True to to automatically open and display the attachment when the alarm is going from Normal to Alarm state.

Object reference

Enter the path to the item you want to attach to the alarm.

  • 报警附件
  • Adding an Attachment to an Alarm
  • Adding an Attachment to Multiple Alarms
  • Removing an Attachment from an Alarm
  • Removing Attachments from Multiple Alarms