Use the Alarm Settings tab to change the alarm properties of an out of range alarm.
Property |
Description |
Acknowledgement type |
Select the type of acknowledgement for the alarm. 有关更多信息,请参阅 Acknowledgements . |
Above upper limit message |
Type the message to display when the variable exceeds the upper limit of the alarm. 有关更多信息,请参阅 Alarm Messages . |
Below lower limit message |
Type the message to display when the variable falls below the lower limit. 有关更多信息,请参阅 Alarm Messages . |
Reset message |
Type the message to display when the alarm is reset. 有关更多信息,请参阅 Alarm Messages . |
Above upper limit priority |
Enter the priority level of the alarm when the variable exceeds the upper limit. 有关更多信息,请参阅 Alarm Priority . |
Below lower limit priority |
Enter the priority level of the alarm when the variable falls below the lower limit. 有关更多信息,请参阅 Alarm Priority . |
Reset priority |
Enter the priority level of the alarm when it is reset. 有关更多信息,请参阅 Alarm Priority . |
Category |
Enter the category the alarm belongs to. 有关更多信息,请参阅 Alarm Categories . |
Category 2 |
Enter the second category the alarm belongs to. 有关更多信息,请参阅 Alarm Categories . |
Cause note group |
Enter the cause note group used by the alarm. 有关更多信息,请参阅 Cause Notes . |
Action note group |
Enter the action note group used by the alarm. 有关更多信息,请参阅 Action Notes . |
Checklist |
Enter the checklist that belongs to the alarm. 有关更多信息,请参阅 Checklists . |
Checklist required |
Select to require that a checklist is filled in before acknowledging an alarm. |
Prefix for alarm source name |
Type a prefix that is added to the beginning of the source name property of an alarm record. |
Disable alarm |
Select to disable the alarm, for example, before deployment. 有关更多信息,请参阅 禁用和启用报警 . |
Auto hide |
Select to automatically hide the alarm in the Alarms pane or Alarm View. 有关更多信息,请参阅 隐藏和显示报警 . |
Disable state-change logging |
Select to prevent an alarm state change from creating an event. 有关更多信息,请参阅 报警状态更改记录 . |
F lashing alert |
Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered. |
Audible alert |
Select to make the alert audible when the alarm is triggered. |
Custom audio |
Enter the path to the custom audio file you want to play when the alarm is triggered. |
|
Edit Click to open the property pane where you edit the selected user action. 有关更多信息,请参阅 Action Note Properties . |
|
Add Click to open the Create Object: Attachment wizard, where you add an attachment. 有关更多信息,请参阅 Create Object Wizard – Naming the Object Page . |
|
Edit Click to open the property pane where you configure the attachment. 有关更多信息,请参阅 Attachment Properties . |
|
Remove Click to remove an attachment that is connected to the alarm. |