earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P Smoke Control, Automation Server Smoke Control, IP-IO Smoke Control, MP-C Smoke Control, MP-V Smoke Control
Functionalities: Smoke Control
Product version: 2022, 2023, 2024, 7.0
5/11/2023

Module and MP Controller Status LEDs

All modules and MP controllers provide a Status LED with different, defined functions as described here.

AS-P/AS Server Status LED

The AS-P/AS Server Status LED indicates its condition as follows:

Table: AS-P/AS Server Status LED Patterns

LED Patterns

AS-P/AS Server Conditions

Green, constant

Normal operation, status OK

Green, flashing (~1 Hz)

Device restarting, wait

Red, constant

Fatal error– attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

Firmware being downloaded, wait

Red/green, vague

Device firmware upgrade mode, wait

Red/green, vague

Reset button has been pressed for more than 8 s, meaning a cold start occurs when the button is released

No light

No input power

PS-24V Power Supply Status LED

The PS-24V Status LED indicates the condition of the device as follows:

Table: Power Supply Status LED Patterns

LED Patterns

Condition

Green, constant

Output voltage and load OK

Red/green, flashing

Output slightly overloaded

Red, constant

Output overloaded

No light

No input power

Central IO Module Status LED

All Central IO modules include a Status LED indicating the condition of the device as described in the following table:

Table: Central IO Module Status LED Patterns

LED Patterns

Center IO Module Conditions

Green, constant

Online and configured (at least one channel/point downloaded successfully)

Green, flashing (200 ms ON, 200 ms OFF)

Online and unconfigured (physical module that either matches/mismatches logical module)

Green, slow flashing (3 sec)

Low power mode (saves energy)

Red, constant

Error requiring attention (for example, the input voltage is too low)

Red, flashing (100 ms ON, 100 ms OFF)

Offline with respect to the AS-P/AS Servers (both configured and unconfigured modules)

Red/Green, flashing (Green 100 ms, Red 100 ms)

Bootloader mode (downloading data)

No light

No input power

MP Controller and IP-IO Module Status LED

All MP controllers and the IP-IO module include a Status LED indicating the condition of the device as described in the following table:

Table: MP Controller and IP-IO Module Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

MP controller firmware application running

Green, flashing (~1 Hz)

Device restarting; wait

MP controller firmware application running

Red, constant

Detected error; attention required

Red, flashing (~1 Hz)

Device is operating but a problem needs attention

Red/green, flashing (~1 Hz)

MP controller I/O board receiving software upgrade; wait

Amber, constant

MP controller firmware boot applet running

Amber, flash

Device restarting; wait

MP controller firmware boot applet started

  • Terminal Base Installation
  • Power Rating
  • PS-24V Power Supply Module
  • Automation Server Installation
  • AS-P and AS-P-NLS Installation
  • Central IO Module Installation