Listed below are the System Alarms with IDs that begin with the letters A-D.
System Alarm ID |
Description |
A configuration error was detected in server communication setup during startup |
A configuration error was detected in one or more server communication setups during startup. |
A log data transfer was missed |
The extended trend may have failed to read records. |
A log sample was missed |
A log sample was missed. |
Alarm signal trigger buffer full |
The alarm is unable to handle all value changes. |
Archive directory does not exist |
The directory path is not valid. |
Archive directory does not exist. Retrying in 5 minutes |
The directory path is not valid. The system will restart the archive process in 5 minutes. |
Archive path must be set to enable archiving |
The destination path for the archive file is not defined. |
Archiving canceled due to configuration change |
The archiving process was canceled due to configuration changes made during the process. |
Archiving failed because of an ongoing operation |
The archiving process failed due to an ongoing operation in EcoStruxure Building Operation software. |
Archiving is not enabled |
Archiving is disabled when a manual archive is initiated. |
System Alarm ID |
Description |
BACnet did not start |
The BACnet communication protocol did not start. This alarm can also apply to Infinet. Be sure to check the path of the alarm to determine whether it refers to BACnet or Infinet. |
BACnet server failure |
There was an internal BACnet error. This alarm can also apply to Infinet. Be sure to check the path of the alarm to determine whether it refers to BACnet or Infinet. |
Bad lead object reference |
Updating shadow object failed because the lead object has an empty type. |
Bad lead object type |
Updating shadow object failed. Type mismatch between lead object and shadow object. |
Blacklisted device detected |
The physical device currently occupying the slot configured for this module has previously reported a Device Address Changed error, and the configuration will not be loaded to the device. Więcej informacji zawiera Device Address Changed . |
System Alarm ID |
Description |
Cannot enable archiving |
The Archiving function is not enabled. |
Cannot verify lead object status |
Updating shadow object failed. Status of the lead object is unknown. |
Communication failed |
Communication failed |
Communication failed Authentication error |
Wrong domain or wrong credentials in server to server communication. |
Communication failed Authorization error |
Insufficient user permissions to communicate with server. |
Communication failed Configuration error |
Server communication failed to start with current communication settings. |
Communication failed Domain is not available |
The requested communication domain is not defined in the server. |
Communication failed Hostname is invalid |
Bad configuration of host name. |
Communication failed Unexpected Server fullpath |
Server path is invalid. |
Communication failed Unexpected Server type |
The server you tried to add is not compatible with the system. |
Communication failed Version Mismatch |
Communication attempt failed between servers with incompatible versions. |
Corrupt backup set is detected |
A corrupt backup set was generated on an Automation server. Backup the server again. |
CWS Alarm Poll failed |
The EcoStruxure Web Services interface failed to poll an alarm from an EcoStruxure Web Services server. |
CWS Browse failed |
The EcoStruxure Web Services nterface failed to browse the database from an EcoStruxure Web Services server. |
CWS GetHistory failed |
The EcoStruxure Web Services interface failed to get a trend log from an EcoStruxure Web Services server. |
CWS GetObject failed |
The EcoStruxure Web Services interface failed to get an EcoStruxure Web Services object from an EcoStruxure Web Services server. |
CWS Method Error |
The EcoStruxure Web Services interface failed while calling an EcoStruxure Web Services method from an EcoStruxure Web Services server. |
CWS Value Poll failed |
The EcoStruxure Web Services interface failed to poll a value from an EcoStruxure Web Services server. |
System Alarm ID |
Description |
|
Database file is corrupt |
A file in the configuration is corrupt. |
|
Database update failed |
There was a failure when trying to save a value or setting. |
|
Device address changed |
The physical IO module detects a change in its communication address, which is likely due to a hardware failure on the IO bus. This alarm requires immediate attention. Więcej informacji zawiera Device Address Changed . |
|
Device offline |
The server cannot connect to the specified device. |
|
Driver loading disabled |
The loading of SmartDriver driver is disabled. Więcej informacji zawiera Load SmartDriver Drivers at Startup . |
|
Driver unexpectedly timed out |
The Automation server software encountered an unexpected problem while trying to communicate with the IO driver of the server. |
|
Duplicate device address |
More than one device has the same MAC address and network ID. |
|
Duplicate device identifier |
There are two or more devices within an interface with the same device identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. Więcej informacji zawiera Unconfigured Devices . |
|
Duplicate device name |
There are two or more devices in a container or network with the same device name. |
|
Duplicate network identifier |
There are two or more networks within an interface with the same Network identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. Więcej informacji zawiera Unconfigured Devices . |
|
Duplicate of local network |
There are two or more networks within an interface with the same Local Network identifier. The system may trigger a system alarm and place the duplicate in the Unconfigured Devices folder. Więcej informacji zawiera Unconfigured Devices . |