Listed below are the System Alarms with IDs that begin with the letters M-NW8 R.
System Alarm ID |
Description |
Module type mismatch |
The module type based on the user’s configuration is different from the type of the actual physical module occupying the same slot. |
More than one server with the same name in the system |
There is more than one EcoStruxure BMS server with the same name in the EcoStruxure BMS. |
System Alarm ID |
Description |
NETWORK 8000 message |
An unknown NETWORK 8000 message with specific included contents was received. |
NETWORK 8000 message end |
End of a NETWORK 8000 unknown message. |
Network offline |
The server cannot connect to the specified network. |
New application program |
The Xenta device has received a new valid application. |
No file name set |
No file name has been specified. |
No valid Blueprint File |
Invalid Xenta device program definition. |
Not enough flash memory for log |
The request was valid but could not be performed because there is not enough flash memory. |
Not enough RAM memory for log |
The request was valid but could not be performed because there is not enough RAM memory. |
Notification files storage capacity reached |
Storage capacity has been reached for notification files. Więcej informacji zawiera Deleting a Notification Written to a File . |