Listed below are the System Alarms with IDs that begin with the letters E-L.
System Alarm ID |
Description |
Email service configuration error |
No email server is specified. |
Email service failed to connect to SMTP server |
The email service failed to connect to the SMTP server. |
Email service failed to login to SMTP server |
The email service failed to log on to the SMTP server. |
Email service failed to send message |
The email service failed to send the message. |
Email service no recipient email address |
There was no recipient to send the email to. |
Email service no sender and recipient email address |
There was no sender email specified and no recipient to send the email to. |
Email service no sender email address |
There was no sender email specified. |
Error in log definition |
Xenta trend log configuration error. |
Error in retrieving Xenta device Trend Log data |
Xenta trend log retrieving error. |
Error - Upgrade using DFU mode |
File system is corrupt. Upgrade using DFU mode. |
System Alarm ID |
Description |
Failed to create object |
The attempt to create an object failed. |
Failed to initialize references |
An object has a reference or binding to a property or another object that cannot be found. |
Failure backing up server database |
A backup operation failed. If the information is available, the server path and technical reason for the failure is supplied in the alarm information. |
Failure restoring server database |
A restore operation failed. If the information is available, the alarm also contains the EcoStruxure BMS configuration path for the server that ran the restore. |
Failure retrieving backup set from remote server |
The Enterprise Server failed to retrieve a newly generated backup set from a SmartX server. The name of the SmartX server is supplied. If the information is available, the file name of the backup set is also supplied. |
File I/O error |
Failed to write to file. |
System Alarm ID |
Description |
Invalid archive path |
The archive path is not valid. |
Invalid archiving format |
The archiving format is not supported. |
Invalid device address |
The device address is not valid. |
Invalid device identifier |
The identifier on the specified device is invalid. |
Invalid license server configuration |
Two or more Enterprise Servers get their licenses from the same license server. This is not the recommended setup. |
IO driver unexpectedly timed out |
The IO driver timed out unexpectedly. |
IO error when generating archive |
There is a detected error during the archive generation. |
IO error when writing to archive temporary |
There is a detected error when the archive is saved to a predefined directory. |
IO error, cannot write to archive directory! |
There is a detected error when the archive is saved to a predefined directory. |
IO error, cannot write to archive directory! Retrying in 5 minutes |
There is a detected error when the archive is saved to a predefined directory. The system will restart the archive process in 5 minutes. |
IO error, not enough space left in the archive directory |
The destination directory does not have enough storage space for the archive. |
IO error, not enough space left in the archive directory! Retrying in 5 minutes! |
The destination directory does not have enough storage space for the archive. The system will restart the archive process in 5 minutes. |
IP connection offline |
Modbus TCP connection timeout. |
System Alarm ID |
Description |
License violation |
The amount of required licenses is greater than the amount of existing licenses on the License Server. |
Local administrator account has empty or default password |
Local administrator account has empty or default password. |
Log full |
The Xenta trend log is full. |
Log stopped because it is full |
The Xenta trend log stopped because it is full. |
Log variable error |
A Xenta trend log variable is missing or invalid. |
Logging started |
The Xenta trend log started logging. |
Logging stopped |
The Xenta trend log stopped logging. |