Listed below are the System Alarms with IDs that begin with the letters NW8 S-NW8 Z.
System Alarm ID |
Description |
NW8 Sensor input failure |
The controller has detected an input sensor range failure. |
NW8 Setpoint out of range |
The Flo2 Remote Setpoint is enabled and out of range. |
NW8 System fault 32 |
Missing changeover input for an MnHpfc fan coil application. |
System Alarm ID |
Description |
NW8 UI diagnostic |
The measured input value at UI:xx (from UI:1 to UI:8) is outside the standard range for the configured sensor for a MICROZONE II controller. |
NW8 Unrecognized command |
The controller did not recognize the command. |
System Alarm ID |
Description |
NW8 Zone temperature out of range |
The MicroFol II zone temperature is out of range. |