earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
12/11/2018

Events Pane Context Menu - Event View Settings Submenu

Use the Event View settings submenu to change the way events are presented.

 
action_zoom_plus_stroke Event View settings submenu
Figure: Event View settings submenu

Table: Event View Settings submenu

Command

Description

Edit event filter

Click to open the Select conditions dialog box where you sort the information in the Events pane or an Event View. For more information, see Select Conditions Dialog Box .

Save as standard layout

Click to save the current Events pane or Event View layout as the standard layout for all users and for the Events pane or the specific Event View.

Reset standard layout to factory default

Click to reset the Events pane or Event View standard layout to factory default.

Add/Remove columns

Click to open the Add/Remove columns dialog box to add or remove columns from the Events pane or Event View. For more information, see Add/Remove Columns Dialog Box (Events) .

Properties

Click to open the Event View dialog box to view and edit the properties of the Events pane or Event View. For more information, see Event View Properties .

Edit the style of associated events

Click to open the Event Styles dialog box where you edit the style of a certain event. For more information, see Event Styles Dialog Box .

D etail view

Click to open a detail view for the selected event. For more information, see Alarm and Event Detail View .

  • Events Pane and Event View Customization
  • Events Pane Context Menu
  • Select Conditions Dialog Box
  • Add/Remove Columns Dialog Box (Events)
  • Event View Properties
  • Event Styles Dialog Box
  • Alarm and Event Detail View