Productos AD v2, AD v1
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1
19/11/2020

Connecting AD to Automation Server and a Power Adapter

You connect AD to an Automation Server in order to communicate with EcoStruxure BMS servers over the USB connection. You connect AD to a USB power adapter in order to supply AD with power and to ensure that its battery is charged. You use a USB “Y” cable to connect AD to both an Automation Server and a USB power adapter.

Mostrar más
action_close

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a SmartX AS-P server, SmartX AS-B server, or USB power adapter, but not by an Automation Server.

Communication over a USB Connection

The preinstalled SmartX AD-Link application enables AD v2 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v2 is connected to a SmartX AS-P server or SmartX AS-B server, AD v2 can be powered by the SmartX server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

 
action_zoom_plus_stroke USB connection to a SmartX AS-P server or SmartX AS-B server
Figura: USB connection to a SmartX AS-P server or SmartX AS-B server
Aviso

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

When AD v2 is connected to an Automation Server, AD v2 must be powered by a USB power adapter. The Automation Server does not provide enough power for AD v2. A USB “Y” cable allows you to connect AD v2 to two different devices, an Automation Server and a USB power adapter, to receive data and power respectively. The screen must not be turned on constantly because this may drain the battery.

 
action_zoom_plus_stroke USB connection to an Automation Server and a USB power adapter
Figura: USB connection to an Automation Server and a USB power adapter

Use only Samsung-approved power adapters. Using other power adapters can cause the battery to explode or damage the tablet.

Advertencia Advertencia

HAZARD OF EXPLOSION OR DEVICE DAMAGE

Use only Samsung-approved power adapters.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Advertencia Advertencia

HAZARD OF EXPLOSION OR DEVICE DAMAGE

Use only Samsung-approved power adapters.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

To connect AD to Automation Server and a Power Adapter
  1. Insert the USB type-A connector with the data communication symbol

     
    action_zoom_plus_stroke
    into one of the USB host ports on the Automation Server.

  2. If an Attention message “Unable to find software on your computer that can recognize your device...” appears on AD, ignore the message and tap OK .

  3. Insert the USB type-A connector with the power symbol

     
    action_zoom_plus_stroke
    into the power adapter.

  4. Plug the power adapter into the standard AC power outlet.

  5. Ensure that the screen timeout is configured to automatically turn off the screen when you are not using the device, because the sleep mode is used to fully charge the battery.

  • AD v2 Communication and Power
  • AD v1 Communication and Power
  • Installing the AD v2 Tablet and Frame
  • Installing the AD v1 Tablet and Frame
  • AD Does Not Turn On or Battery Does Not Charge
  • AD Battery Does Not Fully Charge
  • USB Data Communication is Lagging or Data is Lost