earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AD v1
Funcionalidades: Hardware
Versión del producto: 2.0, 2.1, 3.0, 3.1
22/05/2019

AD v1 Communication and Power

AD v1 can use either a wired (USB) connection or a wireless (WiFi) connection to communicate with EcoStruxure BMS servers. AD v1 can be powered either by a SmartX AS-P server, SmartX AS-B server, or USB power adapter, but not by an Automation Server.

Communication over a USB Connection

The preinstalled SmartX AD-Link application enables AD v1 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v1 is connected to a SmartX AS-P server or SmartX AS-B server, AD v1 can be powered by the SmartX server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

 
action_zoom_plus_stroke USB connection to a SmartX AS-P server or SmartX AS-B server
Figura: USB connection to a SmartX AS-P server or SmartX AS-B server
Aviso

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

When AD v1 is connected to an Automation Server, AD v1 must be powered by a USB power adapter. The Automation Server does not provide enough power for AD v1. A USB “Y” cable allows you to connect AD v1 to two different devices, an Automation Server and a USB power adapter, to receive data and power respectively. The screen must not be turned on constantly because this may drain the battery.

 
action_zoom_plus_stroke USB connection to an Automation Server and a USB power adapter
Figura: USB connection to an Automation Server and a USB power adapter

Use only Samsung-approved power adapters. Using other power adapters can cause the battery to explode or damage the tablet.

Advertencia Advertencia

HAZARD OF EXPLOSION OR DEVICE DAMAGE

Use only Samsung-approved power adapters.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Communication over a Wireless Connection

AD v1 can communicate with EcoStruxure BMS servers through a wireless access point (AP), which is connected to the same network as the EcoStruxure BMS servers. When used as a stationary HMI terminal, AD v1 is connected to a USB power adapter to ensure that its battery is charged.

 
action_zoom_plus_stroke Wireless communication and power from a USB power adapter
Figura: Wireless communication and power from a USB power adapter
  • AD v1
  • Hardware Overview
  • Connecting AD to a SmartX AS-P server or SmartX AS-B server
  • Connecting AD to Automation Server and a Power Adapter
  • Connecting AD to a Power Adapter