Use the Xenta Schedule Editor to view or edit Xenta schedules.
Property |
Description |
Interval type |
Select the interval type. |
Start time |
Select the start time for the weekly event if Interval is selected. |
End time |
Select the end time for the weekly event if Interval is selected. |
(Select weekday) |
Select the weekdays the weekly event is to be in service. |
|
Click to delete a weekly event. |
Interval type |
Select the interval type. |
Start date |
Select the start date for the exception event interval. |
Start time |
Select the start time for the exception event. |
End date |
Select the end date for the exception event interval. |
End time |
Select the end time for the exception event. |
(Select weekday) |
Select the weekdays the exception event is to be in service. |
|
Click to delete an exception event. |