earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
14/12/2018

Multi Trend Log List Properties - Basic Tab

Use the Multi Trend Log List Properties - Basic tab to configure the basic properties of the multi trend log list.

 
action_zoom_plus_stroke Multi Trend Log List properties - Basic tab
Figura: Multi Trend Log List properties - Basic tab

Tabla: Multi Trend Log List Properties - Basic Tab

Property

Description

Log space (records)

​Select the maximum number of records to display in the list.

Show events

Select True to display events in the list. Selecting False does not hide events in the list that contain a value or comment. For example, when a record is added, edited, or commented.

Time zone

Select the time zone in which the log records are presented.

Calculation method

Select a calculation method.

Para obtener más información, consulte Métodos de cálculo .

Delta over period

Select True to apply a period to the delta calculation method.

Para obtener más información, consulte Métodos de cálculo .

Period

Select the time span for which the calculation method is to be executed.

Custom period

Enter a custom time span for which the calculation method is to be executed.

Custom period alignment

Enter the time when you want the custom period to start.

 
action_zoom_plus_stroke

Add

Click to add a series to the multi trend log list. Para obtener más información, consulte Create Trend Chart Wizard – Configure Trend Log Series Page ..

 
action_zoom_plus_stroke

Edit

Click to edit a selected series.

 
action_zoom_plus_stroke

Remove

​Click to remove a selected series.

  • Multi Trend Log Lists
  • Time Zone Modes in a Trend Log List
  • Métodos de cálculo
  • Create Object Wizard – Naming the Object Page
  • Create Trend Chart Wizard – Configure Trend Log Series Page
  • General Information Properties – Basic Tab
  • References Tab