You create a multi trend log list to display values from multiple trend logs in one list so that you can compare the values, for example, when commissioning or validating an EcoStruxure BMS.
In WorkStation, in the System Tree pane, select the location where you want to create the multi trend log list.
On the File menu, point to New and then click Trend .
In the Create Object wizard, in the object type list, select Multi Trend Log List .
In the Name box, type a name for the multi trend log list.
In the Description box, type a description for the multi trend log list.
Click Next .
In the Configure Multi Trend Log List page, in the Log space (records) box, enter the maximum number of rows to display in the multi trend log list.
In the Series box, click the Add button
In the Name box, type a name for the trend series based on the added trend log.
In the Description box, type a description for the trend series.
Click Next .
In the Display trend log box, enter the path to the trend log you want to add to the multi trend log list.
Click Create .
In the Series box, click the Add button
In the Series box, select a trend series and then click the Edit
In the Series box, click the Remove
Click Create .
The multi trend log list displays values from the trend logs you have added to the multi trend log list.