earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Time Zone Modes in a Trend Log List

arrow1_rotationLocal Time Zone arrow1_rotationServer Time Zone arrow1_rotationUTC Time Zone

​In a trend log list, you can present the records of a trend log in different time zones: local time zone, EcoStruxure BMS server time zone, and UTC time zone.

Local Time Zone

Use local time zone to display the trend logs in real time from the perspective of the client.

For example, a trend log in Moscow is monitored on a client in Tbilisi. The trend log is recording at 8:00-13:00 local server time. 13:00 Moscow time is 14:00 Tbilisi time, so the Tiblisi trend log displays 9:00-14:00 in the client trend log list.

 
action_zoom_plus_stroke Trend log list displayed on a client with local time zone.
图: Trend log list displayed on a client with local time zone.

Server Time Zone

Use server time zone to display in real time from the perspective of the EcoStruxure BMS server.

For example, a trend log in Moscow is monitored on a client in Tbilisi. The trend log is recording at 8:00-13:00 local server time and this is how it is displayed in the client trend log list.

 
action_zoom_plus_stroke Trend log list displayed on a client with server time zone.
图: Trend log list displayed on a client with server time zone.

UTC Time Zone

Use UTC time zone to display the trend logs in the perspective of UTC.

For example, a trend log in Moscow is monitored on a client in Tbilisi. The trend log is recording at 8:00-13:00 local server time. 8:00 Moscow time is 5:00 UTC time, so the Tiblisi displays 5:00-10:00 in the trend log list.

 
action_zoom_plus_stroke Trend log list displayed on a client with UTC time zone.
图: Trend log list displayed on a client with UTC time zone.
  • Trend Log Lists
  • Trends Overview
  • Configuring the Trend Log List Time Zone