earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, ​License Administrator, ​License Server, AS-P, WorkStation, WebStation
Functionalities: Basic Functionality, Engineering, License Management
Product version: 3.3, 2022
7/23/2021

License Enforcement

arrow1_rotationLicense Violation

License enforcement is the process of checking whether a software application has a valid license available to it at runtime. If you do not have enough licenses, a license violation occurs. This is accomplished by a license violation bar in WorkStation and WebStation.

If a client, such as WorkStation or one of the editors, attempts to start and cannot locate an available license, the client does not start.

For more information, see EcoStruxture Building Operation Software and Features that Require Licenses .

License Violation

The first time you add an additional device to the Enterprise Server, other than an automation server, in excess of the amount of licenses purchased, a license violation bar is displayed. The license violation bar states that you have exceeded the amount of licenses available, and urges you to purchase the additional licenses required. The license violation bar displays every time you log on to the system, and is displayed on all WorkStations and WebStations that are logged into the system.

The system information alarm, License Violation, is triggered at the same time as the License Violation bar is displayed.

To get more specific information regarding the licenses, you can click on Licensing Information. For more information, see License Information Enterprise Server .

 
action_zoom_plus_stroke License violation bar in WorkStation
Figure: License violation bar in WorkStation

For more information, see License Violation Bar .

  • EcoStruxure Building Operation Software Licensing Overview
  • License Information Enterprise Server
  • License Violation Bar