earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/18

Create Report Data Wizard - Configure Relative Trend Log Page

Use the Configure Relative Trend Log page to configure the content and the presentation of data in a notification report template.

 
action_zoom_plus_stroke Configure Relative Trend Log page
图: Configure Relative Trend Log page

表格: Configure Relative Trend Log Page

Component

Description

Name

Type a name for the data type group.

Relative to

Enter the object with the relation to the notification report template that you want to use as a template for where notification reports are generated.

Relative log path

Add the trend log in relation to the 'Relative to' property.

Record template

Enter the text or substitution codes you want to use in the notification report.

Quick filter

Enter a word to filter on. 有关更多信息,请参阅 Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

Record delimiter

Enter any printable character, space, or a new line feed that you want to use to separate the trend log records in the notification report.

Preview

Use to view how the properties or trend log records appear in the notification report text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

Number of records

Enter the maximum number of trend log records you want to display in the notification report.

  • Notification Reports
  • Trend Logs Substitution Codes
  • Quick Filter
  • Create Report Data Wizard - Configure Properties Page
  • Create Report Data Wizard - Configure Relative Properties Page
  • Create Report Data Wizard - Configure Trend Log Page