earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/18

Create Report Data Wizard - Configure Relative Properties Page

Use the Configure Relative Properties page to configure the content and the presentation of data in a notification report template.

 
action_zoom_plus_stroke Configure Relative Properties page
图: Configure Relative Properties page

表格: Configure Relative Properties Page

Component

Description

Name

Type a name for the data type group.

Relative to

Enter the object with the relation to the notification report template that you want to use as a template for where notification reports are generated.

Properties

Use Properties to add, edit, or remove properties in the data type group.

 
action_zoom_plus_stroke

Add  

Click to add properties to the notification report template.

 
action_zoom_plus_stroke

Edit  

Click to edit the selected property.

 
action_zoom_plus_stroke

Remove  

Click to remove the selected property from the notification report template.

Property template

Enter the text or substitution codes you want to use in the notification report.

Quick filter

Enter a word to filter on. 有关更多信息,请参阅 Quick Filter ..

Substitution codes list

Add the substitution codes you want to use in the notification or notification report.

Property delimiter

Enter any printable character, space, or a new line feed that you want to use to separate the properties in the notification report.

Preview

Use to view how the properties or trend log records appear in the notification report text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

  • Notification Reports
  • Properties Substitution Codes
  • Quick Filter
  • Create Report Data Wizard - Configure Properties Page
  • Create Report Data Wizard - Configure Relative Trend Log Page
  • Create Report Data Wizard - Configure Trend Log Page