earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 3.2, 3.3, 2022
4/15/2021

Create Object Wizard - Configure Write to File Page

Use the Configure Write to File page to configure the write to file properties of the notification.

 
action_zoom_plus_stroke Configure Write to File page
Figure: Configure Write to File page

Table: Configure Write to File Page

Component

Description

File name

Type a name for the file.

Overwrite

Select True to overwrite the file when a new file is generated.

 
action_zoom_plus_stroke

Click to open the Configure dialog box where you configure a reference for a dynamic file name. For more information, see Configure Dialog Box – Configuration Tab .

Uniquenes s

Select whether to append or prepend a timestamp to the file name, or generate the file without any timestamp. The timestamp in the file name is expressed in UTC.

Convert to PDF

Select True to convert your notification report to PDF format.

Sign PDF

Select to sign your PDF. Signing of PDF reports will require license. If no valid license is available, the PDF report is generated, but not signed. A red text will be visible on top of the report.

PDF paper size

Select the size of paper to be used for display and print.

PDF page orientation

Select the orientation of page in display and print.

  • Notification Distribution Methods
  • Document Signature Certificate
  • Creating an Alarm Triggered Notification
  • Configuring an Alarm Triggered Notification 
  • Creating a Variable Triggered Notification
  • Configuring a Variable Triggered Notification
  • Signing a PDF Notification Report with a Certificate
  • Alarm Triggered Notification View
  • Variable Triggered Notification View
  • Configure Dialog Box – Configuration Tab
  • EcoStruxure Building Operation Software Licensing Overview