earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2023
12/16/2022

Alarm Triggered Notification View

Use the Alarm Triggered Notification view to view and edit the configuration of an alarm triggered notification.

 
action_zoom_plus_stroke Alarm triggered notification view
Figure: Alarm triggered notification view

Table: Alarm Triggered Notification View

Number

Description

 
action_zoom_plus_stroke

Properties

Use the properties to configure how the notification is activated, what notification report to connect to the notification, and what properties to use for the notification text. For more information, see Alarm Triggered Notification Properties - Basic Tab ..

 
action_zoom_plus_stroke

Notification text

Use the notification text to edit the contents and formatting of the notification text. For more information, see Notifications ..

 
action_zoom_plus_stroke

Quick filter

Use the Quick filter to enter a word to filter on. For more information, see Quick Filter ..

 
action_zoom_plus_stroke

Substitution codes list

Use the alarm substitution codes list to select the data you want to include in the notification. For more information, see Alarms Substitution Codes ..

 
action_zoom_plus_stroke

Distribution method

Use the distribution method to start a wizard where you configure how the notification is distributed.

For more information, see Create Object Wizard - Configure Email Page .

For more information, see Create Notification Wizard - Configure SNMP Page .

For more information, see Create Object Wizard - Configure Write to File Page .

 
action_zoom_plus_stroke

Filter Settings

Use the filter settings to select the alarm filter conditions that have to be met before the notification is triggered. For more information, see Alarm Filters ..

  • Notifications
  • Create Object Wizard – Configure Alarm Triggered Notification Page
  • Alarm Triggered Notification Properties - Basic Tab
  • Notification Reports
  • Quick Filter
  • Alarms Substitution Codes
  • Create Object Wizard - Configure Email Page
  • Create Notification Wizard - Configure SNMP Page
  • Create Object Wizard - Configure Write to File Page
  • Alarm Filters