Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Alarm Triggered Notification View

Use the Alarm Triggered Notification view to view and edit the configuration of an alarm triggered notification.

 
action_zoom_plus_stroke Alarm triggered notification view
Rysunek: Alarm triggered notification view

Tabela: Alarm Triggered Notification View

Number

Description

 
action_zoom_plus_stroke

Properties

Use the properties to configure how the notification is activated, what notification report to connect to the notification, and what properties to use for the notification text. Więcej informacji zawiera Alarm Triggered Notification Properties - Basic Tab ..

 
action_zoom_plus_stroke

Notification text

Use the notification text to edit the contents and formatting of the notification text. Więcej informacji zawiera Notifications ..

 
action_zoom_plus_stroke

Quick filter

Use the Quick filter to enter a word to filter on. Więcej informacji zawiera Quick Filter ..

 
action_zoom_plus_stroke

Substitution codes list

Use the alarm substitution codes list to select the data you want to include in the notification. Więcej informacji zawiera Alarms Substitution Codes ..

 
action_zoom_plus_stroke

Distribution method

Use the distribution method to start a wizard where you configure how the notification is distributed.

Więcej informacji zawiera Create Object Wizard - Configure Email Page .

Więcej informacji zawiera Create Notification Wizard - Configure SNMP Page .

Więcej informacji zawiera Create Object Wizard - Configure Write to File Page .

 
action_zoom_plus_stroke

Filter Settings

Use the filter settings to select the alarm filter conditions that have to be met before the notification is triggered. Więcej informacji zawiera Alarm Filters ..

  • Notifications
  • Create Object Wizard – Configure Alarm Triggered Notification Page
  • Alarm Triggered Notification Properties - Basic Tab
  • Notification Reports
  • Quick Filter
  • Alarms Substitution Codes
  • Create Object Wizard - Configure Email Page
  • Create Notification Wizard - Configure SNMP Page
  • Create Object Wizard - Configure Write to File Page
  • Alarm Filters