Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2021-04-15

Create Object Wizard - Configure Write to File Page

Use the Configure Write to File page to configure the write to file properties of the notification.

 
action_zoom_plus_stroke Configure Write to File page
Rysunek: Configure Write to File page

Tabela: Configure Write to File Page

Component

Description

File name

Type a name for the file.

Overwrite

Select True to overwrite the file when a new file is generated.

 
action_zoom_plus_stroke

Click to open the Configure dialog box where you configure a reference for a dynamic file name. Więcej informacji zawiera Configure Dialog Box – Configuration Tab .

Uniquenes s

Select whether to append or prepend a timestamp to the file name, or generate the file without any timestamp. The timestamp in the file name is expressed in UTC.

Convert to PDF

Select True to convert your notification report to PDF format.

Sign PDF

Select to sign your PDF. Signing of PDF reports will require license. If no valid license is available, the PDF report is generated, but not signed. A red text will be visible on top of the report.

PDF paper size

Select the size of paper to be used for display and print.

PDF page orientation

Select the orientation of page in display and print.

  • Notification Distribution Methods
  • Document Signature Certificate
  • Creating an Alarm Triggered Notification
  • Configuring an Alarm Triggered Notification 
  • Creating a Variable Triggered Notification
  • Configuring a Variable Triggered Notification
  • Signing a PDF Notification Report with a Certificate
  • Alarm Triggered Notification View
  • Variable Triggered Notification View
  • Configure Dialog Box – Configuration Tab
  • EcoStruxure Building Operation Software Licensing Overview