AS-B has the following communication ports:
2 Ethernet 10/100 megabit ports
1 RS-485 port
1 USB host port
1 USB device port
Communication port |
Connection |
Ethernet 1 10/100 |
IP, LAN/WAN, Modbus, BACnet |
Ethernet 2 10/100 |
IP, LAN/WAN, Modbus, BACnet |
RS-485 |
Modbus, BACnet |
USB host |
Advanced Display (AD), Wireless Adapter - Advanced |
USB device |
Device Administrator |
The Ethernet communication is performed over a 10/100BaseTX, 10 or 100 Mbit/s, twisted pair network. The AS-B servers have two Ethernet ports with RJ45 connectors.
The two Ethernet ports can be configured in three different modes: switching enabled, second port disabled, or dual IP networks. One port should be connected to the site network. When switching between the two ports is enabled, the other port can be used to connect computers running WorkStation or WebStation, Modbus TCP units, or BACnet/IP devices such as MP controllers, but not another EcoStruxure BMS server. To limit access to the system, you can disconnect the second port. When the two ports are configured in dual IP mode, you can connect a separate network of IP devices to the second port. The automation server has the option to act as a DHCP server on this network. You can lock the DHCP network and only allow current DHCP clients to communicate with the automation server.
The USB host port can be used for connecting devices such as the Advanced Display (AD) and Wireless Adapter - Advanced. Para mais informações, consulte Connecting AD v3 to an Automation Server and a 24 VAC or 24 VDC Power Supply .Para mais informações, consulte Wireless Adapter - Advanced .
The USB device port is intended for program download from a PC by means of Device Administrator. The port is connected to a PC or a downstream port of a hub.